energy chain
Energy and data transmission rolled out and connected in under 60 minutes A new energy chain system for intralogistics and crane systems has been designed by motion plastic experts igus. The company, whose UK headquarters are in Northampton, has designed and manufactured the ‘autoglide 5 system’, a unique product which guides energy safely, for long […]
The hybrid energy chain YE is a combination of both lightweight plastic and tough steel. It was developed to meet the requirements of construction machinery and lifting equipment, which have high unsupported travels. To watch the video showing how easy it is to add the YE.42 hybrid energy chain to a Cherry Picker please visit https://youtu.be/7dkUJ6LcMnM […]
Lubrication-free tribo-polymers ensure the reliable operation of vertical farming systems. Motion plastics from igus are playing a major role in the increasingly popular sector of vertical farming. igus, which has its UK headquarters in Northampton, is working closely with global companies specialising in vertical farming – the practice of growing plants indoors in stacked layers […]
The e-loop energy supply series which increases safety and reduces procurement and installation time has been expanded to suit static applications, including shore power supplies. Shore power offers the provision of electrical power to a ship at berth so that its main and auxiliary engines can be shut down. Stricter guidelines are forcing ports to implement more environmentally […]
A frequently asked question is whether additional cables can be attached to igus® Robolink DP. The answer is yes! In this week’s video of the week you can see how this is possible. You can now use the new triflex® TR.30 KIT, which is simple to install, providing additional cables on the Robolink DP if […]
6th August, 2020 In order to supply modern motors with energy and data, users need appropriate cables that function reliably, even at high accelerations and on long travels. Especially for dynamic use, igus has now developed a hybrid cable that is offered as a drive solution for the new Bosch Rexroth motors. It combines an […]
17th July, 2020 The igus® e-skin® is a modular corrugated tube developed for use as a flat cable guidance system for cleanrooms. These energy chains supply cleanroom machines with data, media and energy. The zipper design is easy to open and close making cable installation simple. The e-skin® chain comes in 3 different types and various […]
26th June, 2020 The innovative Camping Butler cleans mobile toilet cartridges, from caravans and camper vans, fully automatically and contact-free from the inside and outside. No matter how full or very dirty the cassette is, the Camping Butler cleans it completely. In the week’s video, we go behind the scenes to see how exactly the […]
16th June, 2020 The new e-spool flex from igus moves a single cable or hose safely and stows it away quickly whilst retaining an end-to-end connection. This increases safety at manual workstations and on control pendants. The spiral guide allows quick installation of the cable into the reel and the e-spool flex is ready for […]
3rd June,2020 As scientists delve into the study of climate change, new strategies and products are evolving to help them uncover data that is driving the world’s foremost crisis. The scientific community is obtaining significant information from international oceans, especially with the support of autonomous surface vehicles. Igus provided data cables and energy chains to […]