e-chain
Plastics expert igus has developed the world’s first ‘e-skin flat’ single pod – designed specifically to guide cables in compact and particle-free cleanrooms. To ensure quick and easy installation customers can use the e-skin flat to select and combine chambers and then insert the cables in seconds. There is also the option of a new […]
Energy and data transmission rolled out and connected in under 60 minutes A new energy chain system for intralogistics and crane systems has been designed by motion plastic experts igus. The company, whose UK headquarters are in Northampton, has designed and manufactured the ‘autoglide 5 system’, a unique product which guides energy safely, for long […]
The hybrid energy chain YE is a combination of both lightweight plastic and tough steel. It was developed to meet the requirements of construction machinery and lifting equipment, which have high unsupported travels. To watch the video showing how easy it is to add the YE.42 hybrid energy chain to a Cherry Picker please visit https://youtu.be/7dkUJ6LcMnM […]
The e-loop energy supply series which increases safety and reduces procurement and installation time has been expanded to suit static applications, including shore power supplies. Shore power offers the provision of electrical power to a ship at berth so that its main and auxiliary engines can be shut down. Stricter guidelines are forcing ports to implement more environmentally […]
12th August, 2020 Side-mounted energy chain from igus ensures reliable energy supply in high-speed lightweight linear robots Twice as fast at half the weight: this is what makes the linear motor robot from FIBRO LÄPPLE TECHNOLOGY (FLT) different from many other solutions. In order for the linear robot to be able to get production up […]
6th August, 2020 Brickworks are very harsh environments for any product, from the extreme dust and aggressive dirt to the high loads and fluctuating temperatures. igus® energy chains protect the encapsulated cables whilst continuing to meet the high demands of the application. These chains endure severe conditions but thanks to their reinforced configuration this has […]
17th July, 2020 The igus® e-skin® is a modular corrugated tube developed for use as a flat cable guidance system for cleanrooms. These energy chains supply cleanroom machines with data, media and energy. The zipper design is easy to open and close making cable installation simple. The e-skin® chain comes in 3 different types and various […]
26th June, 2020 The innovative Camping Butler cleans mobile toilet cartridges, from caravans and camper vans, fully automatically and contact-free from the inside and outside. No matter how full or very dirty the cassette is, the Camping Butler cleans it completely. In the week’s video, we go behind the scenes to see how exactly the […]
16th June, 2020 The new e-spool flex from igus moves a single cable or hose safely and stows it away quickly whilst retaining an end-to-end connection. This increases safety at manual workstations and on control pendants. The spiral guide allows quick installation of the cable into the reel and the e-spool flex is ready for […]
26th May, 2020 Being able to predict and plan maintenance is the goal pursued by igus with its smart plastics solutions. Intelligent sensors, for example, measure the wear of energy chains, chainflex cables, slewing rings and linear guides. With the new icom.plus communication module, the customer can now decide in which form they would like […]