lubrication-free
Grease is a thing of the past! It’s the dirty and costly way of lubricating your bearings and moving parts. In the future it will be outed as the combustion engine of the mechanical work and users will be searching for that new and efficient way of keeping production lines and other equipment running. You […]
Lubrication-free igus plain bearings allow new, go-anywhere electric stand-up vehicle to operate in even the most difficult environmental conditions An electric version of man’s most dependable and versatile friend, the horse, is now a reality. Canadian company LyteHorse Labs has designed a novel all-terrain electric vehicle, suitable for many applications and environmental conditions. igus bearings […]
Have you ever considered all the applications where things turn? There are thousands!! And to help these applications turn with a smooth motion, customers are using the igus® PRT slewing ring bearing. These bearings are low-cost, maintenance free and require no lubrication! In this weeks’ video of the week, the PRT shows the ease to […]
Lubrication-free and maintenance-free high-load material iglidur TX2 demonstrates 3.5-fold improved wear performance in tests. Especially forhigh-load applications in the construction, machinery, or agricultural industries, igus can now offer the new Tribo (tribologically optimized) material iglidur TX2, which works without lubrication. Even smaller excavating machines still need about 50 litres of lubricant per year with metal […]
igus experts present how motion plastics can reduce costs and sustainably improve technology in a series of live shows Our mobility is changing rapidly: e-scooters, e-bikes, e-cars and vehicles with alternative power sources are increasingly common. The concept of car sharing is also establishing itself in cities worldwide. At the IAA Mobility Show 2021 in […]
In this week’s video of the week, It is all about drylin®! To celebrate the new drylin® product information webpages, this week’s video highlights all the key benefits of using drylin® over alternatives. The lightweight, dirt resistant, sustainable linear systems sell themselves. To view the video, click here https://youtu.be/qOOYXw0Z1DY For more information on the drylin® […]
New bearings made of iglidur W360 high-performance plastic ensure precise and easy linear movements The new iglidur W360CM series linear bearings are designed to slide on round shafts with high precision. The linear bearing consists of an aluminium housing and a polymer liner, which ensures high accuracy. The design allows precise movement. By using iglidur […]
The space-saving PRT-04 slewing ring bearings are now available in a range of sizes with inner and outer tooth drives and a locking function. Compact and lightweight, the new bearings have been developed specifically for movement in tight spaces and give igus an entire PRT-04 modular system. The lubrication-free, slewing ring bearing system comes in […]
The manus award- igus’s awards programme for polymer bearing applications, received 582 entries in 2021. Back in 2019, The iFLY15 catamaran won silver in the manus awards and is now attempting to break a world record. Twin-hulled catamarans are designed to lift out of the water on hydrofoils, and the iFLY15 sports catamaran from CEC […]
Lubrication-free tribo-polymer iglidur I8-ESD enables the cost-effective manufacture of durable special parts with no minimum order quantity For safe and reliable production in the electronics and semiconductor industry, components are required that have electrostatically conductive properties. This is because even a small electric shock can destroy expensive production lines. igus has now developed a new […]